AnsweredAssumed Answered

E5052B phase noise measurement above 60GHz

Question asked by NCCU1990 on Nov 24, 2009
Latest reply on Oct 2, 2019 by tristanren
Dear Sir:

I want to do the 65GHz phase noise measurement at E5052B,
but I have some PN test issue is unclear.

1. How  can I make sure that the 11970V harmonic mixer is working well?
2. Are E5052B compensate any harmonic mixer data into test result?
3. Is 11970V harmonic mixer have the phase noise information?
4. How can I know that LO input will effect the PN measurement?

Thank you.  

Outcomes