AnsweredAssumed Answered

Phase noise measurement using A3.03 E5500 software

Question asked by Pulse.Analyzer on May 22, 2009
Latest reply on May 26, 2009 by RayH
Why can't I select a 1 Hz offset when doing Single Sideband Phase Noise on an 8662A ?
After entering the marker at 1 Hz it automatically selects .9375 Hz . If I move the marker the next selectable point is 1.0175 Hz or there about.

The only way I can tell what 1 Hz offset is is to redraw the graph so that its 0.5 Hz to 2 Hz with upper limit and lower limit a range of about 20 and eyeball the measurement.

Software is E5500 version A 3.03
System is E5504B with 8257 generator I think and the Z divider.

Is there a way to have the software interpolate this value?

Thanks,  

Outcomes