AnsweredAssumed Answered

E5052B - Retrieving data

Question asked by samTAS on Jul 7, 2008
Latest reply on Jul 21, 2008 by samTAS
Hello,

I have a E5052B SSA which is driven by a GPIB controller on my PC.
What I'm trying to program is :

- Displaying a trace in the X interval [100Hz - 100kHz]
- Using CALC.PN1.TRAC1.DATA.FDAT? to retrieve samples displayed on the screen.

Here is the problem I have :

I need to retrieve samples from 300Hz to 20kHz, but I get all samples
from the display interval.

Do you think it's possible to retrieve only what I want with this command or another one ?

Thanks in advance for your help.  

Outcomes