I want to choose the proper power supply for 346b, what are the critical specs of the supply I should pay attention? Are there special supplies for noise sources?
About the 346b noise source, i have a spectrum analyzer hp8560 in my lab. How can i see the output of 346b on the spectrum. I don't want to make precise measurement, just to see if the 346b responds with 28Vdc supply.
current is 60ma peak
the noise sources have an internal regulator board, so there are no special requirements for the power supply. Any regular lab supply should be OK.
there are no special power supplies for noise sources.