AnsweredAssumed Answered

Collect data as fast as possible

Question asked by capngene on Dec 22, 2010
I want to get a continuum of the amplitude of the center frequency data to a computer as fast as possible for display in the computer program. I don't need any other information. Other than DISPLAY OFF is there any other commands I should be using? I can't use zero span because the drift of my generator is a few hundred kHz, so I'm using a very narrow span and a large video bandwidth to make the generator drift relatively insignificant wrt the center frequency amplitude.  

Outcomes