AnsweredAssumed Answered

Analysis Bandwidth

Question asked by WadeW on Dec 12, 2007
Latest reply on Jan 4, 2008 by mmazooji
I am using MXA with 25MHz BW option along with 89600 (running on the MXA). I set up the 89600 SW for digital demod and attempt to set BW to 25 MHz (by clicking 'max span' and entering manually) and it defaults me back to some odd span of approximately 15MHz (15.165 MHz or something). How do I set up for 25MHz span capture/demod using MXA and 89600?

(FYI, my CF is 100MHz, demod is QPSK, all other settings at default, I am using 89600 version 7.0 and have latest version firmware in the MXA).  

Outcomes