Hi,
I am using N1996A spectrum analyzer and am controlling it via LAN.
I have set the Center frequency with: ":SENS:FREQ:CENT 2407 MHZ\n"
I have set the Span Frequency with: ":SENS:FREQ:SPAN 20 MHZ\n"
I have selected the Reference level with: "DISP:WIND:TRAC:Y:RLEV 20dBm\n"
I have selected the Bandwidth with: "BAND:RES 3MHz\n"
Now I need to set the Ext Gain; how? (on keyboard: AMPTD --> More 2 of 2 --> Ext Gain --> -22 db)
and set the Marker1 at some frequency; how? (on keyboard: MARKER --> 2407 MHz)
and read the value at the marker; how?
any help appreciated. thanks.
I am using N1996A spectrum analyzer and am controlling it via LAN.
I have set the Center frequency with: ":SENS:FREQ:CENT 2407 MHZ\n"
I have set the Span Frequency with: ":SENS:FREQ:SPAN 20 MHZ\n"
I have selected the Reference level with: "DISP:WIND:TRAC:Y:RLEV 20dBm\n"
I have selected the Bandwidth with: "BAND:RES 3MHz\n"
Now I need to set the Ext Gain; how? (on keyboard: AMPTD --> More 2 of 2 --> Ext Gain --> -22 db)
and set the Marker1 at some frequency; how? (on keyboard: MARKER --> 2407 MHz)
and read the value at the marker; how?
any help appreciated. thanks.
Remote Command [:SENSe]:CORRection:OFFSet[:MAGNitude] <rel_ampl>
[:SENSe]:CORRection:OFFSet[:MAGNitude]?
[:SENSe]:CORRection:OFFSet[:MAGNitude]:STATe OFF|ON| 0|1
[:SENSe]:CORRection:OFFSet[:MAGNitude]:STATe?
Example :CORR:OFFS 10.0
:CORR:OFFS:STAT ON
Marker X command:
Remote Command :CALCulate:MARKer[1]|2|3|4:X <real>
:CALCulate:MARKer[1]|2|3|4:X?
SCPI Example: CALC:MARK3:X 1GHz activates the Marker3 and positions it on the
trace at 1 GHz.
Marker Y command:
Remote Command :CALCulate:MARKer[1]|2|3|4:Y?
SCPI Example CALC:MARK2:Y?
All of the above commands are in the User's and Programmer's manual: http://cp.literature.agilent.com/litweb ... -90019.pdf