AnsweredAssumed Answered

why can't I change the wavelength of 81950A?

Question asked by jillar on May 9, 2011
Latest reply on May 10, 2011 by mkelly
My 81950A module was in slot3 in 8164B.when I write the command
sour3:wav 1600nm
to it, it has no response and the wavelength remains 1527.5nm, nor can I change it over the machine(after I change it and press ok, it just go back to 1527.5nm).
Could you please help me with that?  

Outcomes