AnsweredAssumed Answered

Compact Tunable Laser 81949A

Question asked by sychong on Dec 4, 2008
Latest reply on Dec 4, 2008 by sychong
Our lab just bought a new set of 8163B Lightwave Multimeter with 81635A Power Sensor Module (installed at Slot1) and 81949A Compact Tunable Laser - Angled contact connector (installed at Slot2). We are using 81000NI FC/APC connector interfaces.

I have few problems as below:
1. The Tunable Laser is not allow me to select the output power that lesser than 4 mW? 

2. The system is also not allow me to change the prefix of power (mW to nW or pW) as I pressed the softkey, although the softkey are function well. 

I did try to change the output power of the laser through Labview also, but it came out the error "Out of the range of 0.003 to 0.029".

Please help me to solve these problems.

Thanks in advance.  

Outcomes