AnsweredAssumed Answered

Error starting Power Measurement Application v. 1.11

Question asked by AndreasK on Jun 16, 2009
Latest reply on Jul 1, 2009 by xkunes
Hello,

I installed the Power Measurement Application on my computer without problems. But if I start it afterwards, it just loads the splash screen and then I receive the following error in a new window box: "Error: Input string was not in a correct format". An oscilloscope (MSO6134A) is connected to the computer via USB and the Agilent IO Control as well as the IntuiLink Data Capture Software are working fine. But what I need is a real time few (and control if possible) of the oscilloscope via the computer.

Does anybody experienced the same problem?

Thank you in advanced.

Best regards

Andreas  

Outcomes