AnsweredAssumed Answered

85629B TAM for use with 8562A

Question asked by jltran on Feb 1, 2010
Latest reply on May 4, 2010 by MikeM
I have an 8562A SA with Opt H51, SN 3148A06969, that is also described as an AN/USM-489A, SN 00518, that I would like to find a TAM for use with in the future.  However, going through the firmware notes in 08560-90163 the serial numbers of compatible 8562A's only goes up to SN '3147A and below' for Rev. E of the 85629B.  Therefore, it would appear that I have a later unit or there was a unique SN sequence for military units.  In any event, will the Rev. E 85629B work with my 8562A?  Is it safe to try?

Thanks,

Joe  

Outcomes