I am using labview to control the N9340B to measure the field strength. What I try to do load data file to trace, load antenna file and read trace back at different format. Can anyone tell me what commands that I should use? I can remotely set parameters such as: "start, stop freq", but had no luck on the file management.
Thank you very much!
Thank you very much!
Currently N9340B doesn’t support file management via SCPI commands. You may need to load the file manually, then use the command “:TRACe1|2|3|4[:DATA]?” to read the trace data.