AnsweredAssumed Answered

Help with an 86130A

Question asked by swperk on Jan 30, 2012
Latest reply on Feb 1, 2012 by mkelly
Hello,

I just acquired an 86130A Error Performance Analyzer that is in pristine condition (and even had the Agilent cal seals intact), but it does not power on when plugged in and the power button is pressed. I hear a relay click when I plug in the line cord, and when I opened it up, I saw a couple of green LEDs illuminated on one of the power controller boards, but there are no other obvious signs of life. The BR2335 Li coin cell on the controller board was dead so I replaced it, but that did not change anything. It looks so clean and well taken care of that I think if I could just get it to power up it would be fine. I am open to any suggestions, pointers, references, etc. on getting this instrument operating.

Thanks,
Stan  

Outcomes