AnsweredAssumed Answered

Using the Average with Infiinium 7104

Question asked by Oscilador on Nov 15, 2011
Latest reply on Nov 16, 2011 by Oscilador
Hi, I´m trying to read an averaged value of an 7104 scope... with the Normal and High resolution modes of acquire, the program (in VEE) works fine, but the mode I want to use is the average because it filters a lot my measurement, but when the program tries to read the values it stop exectuting...

The program is something like this:

WRITE TEXT":RUN"
WRITE TEXT":CDISPLAY"
WRITE TEXT":DIGITIZE"
WRITE TEXT"MEAS:STATISTICS ON"
WRITE TEXT"MEAS:RESULTS?
READ TEXT x REAL64 ARRAY:20


I think I have to wait until the scope performs the number of averages I set but I don´t know how... I tried to put a delay after the MEAS:RESULTS? but nothing... and I repeat that this code works with Normal and High Resolution (because is like a single sweep)

I hope you can help me...
Thanks.  

Outcomes