Hello, I have an HP8563A Spectrum Analyzer that has several issues. At the moment I believe that I have determined that the output from the A21 10 MHz OCXO output is low as the service manual I have says the level at the connector should be 3 V p-p. I have provided an external 10 MHz source to that connector at the correct level, but still do not have 10 MHz being properly distrubuted to each of the connectors as recommended in the manual. The service manuals do not have schematic level circuit diagrams and I do not know where you can get the CLIP's for this analyzer at this point. I have started making my own schematic but this is painstakingly slow.
Does anyone have the schematic or CLIP for the A15 Board? I believe even if you have a CLIP for the HP 8560A, 8562A or 8563A that would be good enough for me to trace through where the problem lies. Thanks in advance for an assistance.
Larry
Does anyone have the schematic or CLIP for the A15 Board? I believe even if you have a CLIP for the HP 8560A, 8562A or 8563A that would be good enough for me to trace through where the problem lies. Thanks in advance for an assistance.
Larry
Welcome to the forum!
Since the product is out of support I wouldn't mind just copying and giving you the pages you would need from my dusty old CLIP if we can figure out which pages you need.
There were several different flavors and many different versions of the A15 board. If you could tell me the part number of the A15 board you have I may be able to locate the correct CLIP set and scan the correct schematics for you.
Each schematic has 4 oversized pages which are hard to scan, so I'd like to make sure it is something you would be able to use before I go through the effort.
Even if I am able to locate them, please be aware that these documents are no longer in support, may be out of date or contain errors, and Agilent will not be able to provide any repair parts.
Best regards,