AnsweredAssumed Answered

Data point extraction from DSO1014A

Question asked by SIPL on May 23, 2011
My requirement is to retrieve data points from the agilent CRO. I am using viScanf function for retrieving data points. I was able to successfully retrieve datapoints as a  character type array. But my actual requirement is to retrieve data into a double(or float) type array.


My main intention  is to know  how to take multiple readings from an instrument(Agilent DSO1014A).


When i was browsing internet i found the following link from National Instruments :
http://zone.ni.com/devzone/cda/tut/p/id/4727#toc1

please go through the "FLOATING POINT SECTION" in the provided link and in the same way anything is possible to extract multiple data points with the help of Agilent DSO1014A

Thanks in advance.

Regards,
NEWUSER  

Outcomes