AnsweredAssumed Answered

U2702A/2701A Samples retrieval

Question asked by rene.campos@continental-corporation.com on Mar 17, 2011
Latest reply on Sep 12, 2011 by jmobrien
I am doing a DLL for TxSl 5.1 to capture some data and analyse it.  I am using the AgU2701A.dll to communicate through IVI-COM.

I can do the Init Reset and close Ok.

I also can capture the 1250 samples with the function ReadWaveform(50000, &WaveformArray, pInitialX, pXIncrement); I can get the 32M samples with the function ReadFullWaveform(&Data, pLength);

The problem resides in the fact that I need more than the 1250 samples that I can obtain with the first function, and that if I use the second function I will take too long to download so many samples, and I am only using 200K samples.

Is there a way around this? letting the scope know I only need an specific number of samples so I just download that specific number and not the 32M  and then discard 99.375% of the obtained data?



Best Regards,

Rene  

Outcomes