AnsweredAssumed Answered

Problem powering on 8565EC Spectrum Analyzer

Question asked by Matt on May 17, 2007
Latest reply on May 18, 2007 by BobNelson
During power up, my 8565EC Power LED blinks and I can hear an audible switching sound from the unit.

The display remains blank during as if the unit was not powered up.

I have tried different outlets and power cords. I have checked the line voltage switch and the fuse.

I also called to the Agilent help desk for assistance, but the representative was unable to help me at the time.

Has anyone heard of a problem like this.

Thanks.  

Outcomes