I am using ADS2011.05 in a XP 64 bits WS and I try to define a slotline in a multilayer substrate. When the slot is defines in the first metalization layer I can see on with the 3D EM Preview option the correct structure. but if I define as slot an other metalization layer I cant see with the preview option this layer. There are anyone that knows what I am doing wrong?