AnsweredAssumed Answered

bodw + DAC + layout generation

Question asked by DAVID.DENIS on Oct 30, 2008
Hello,

Trying to construct a wirebond array from a text file. I'm using a DAC to set the gap parameter for example. It simulates ok. But I cannot generates the layout view automatically:

"Item: BONDW1 From Design: .../dac_wire
Cannot load component artwork.

If variables are used for parameter values, be sure to define the variables in the VAR component.
Or use Options>Variables to reference another design that contains the variables
BONDW1 WIRESET1  (in Schematic)
Failed to generate artwork"


Is there a workaround available?

Regards,
David  

Outcomes