Is there a way in ADS to simulate a radiating electromagnetic source? For example an isotropic radiating source and in a distance of 10meters a sink antenna at which a voltage probe measure the received voltage.???
ADS has channel models with fading which allow you to set up some antenna problems as you describe using behavioral parameters. But there is no physical, EM based model. You'd have to model those using Momentum or other EM simulators.