Hello to all!
Is this right: the momentum simulation of a one Dipole antenna returns reflection coefficient s11 and characteristic impedance of the antenna Z0 (modeled as transmission line).
The input impedance of the antenna is:
Zant = Zport* (1+S11)/(1-S11).
Thanks for post.
Harald :-/
Is this right: the momentum simulation of a one Dipole antenna returns reflection coefficient s11 and characteristic impedance of the antenna Z0 (modeled as transmission line).
The input impedance of the antenna is:
Zant = Zport* (1+S11)/(1-S11).
Thanks for post.
Harald :-/
Is there something else to mind to?
Thanks for support.
I have a question about Gerber file format and I would appreciate you help.
I want to import a layout with the .GBR extension to Circuitcam software to fabricate a lange Coupler
However,the layout is not properly exported the spacing between the finger of lange coupler vanishes.My Question is
How can I import a .GBR file to Circuit CAM?