AnsweredAssumed Answered

Create Layout Objects from external application

Question asked by Chemic on Sep 30, 2009
Hi,

For my work I developed some simple programs to calculate the dimension of certain Microwave components authomatically.
I am searching a way to link this directly to ADS, in order to skip the "copy and paste" procedure that is extremely long and error prone.
The options I am considering are either to create an *.dsn file to open directly in Momentum or to create AEL programs that can read the design dimensions and draw the components directly in Momentum.

The problems I encounter are

1) there is no specification of the layout *.dsn file
2) I don't understand, even from the AEL support documentation, what functions to use to draw forms in Momentum (if that is possible)

Do you have any hint, link or documentation on this?

Thanks a lot.

S.  

Outcomes