Can I create FET models in MOM?If I have the FET's s2p files or samll signal model ,how can I simulate it with others passive layout component together? or MOM can only simulate passive circuits? Thanks! -cqcq
Momentum only simualtes passive structures, and what some engineers have done is to model the interconnect up to the active device (gate/etc. electrodes) and then combine the active model with the passive parasitic structure. However, usually the parasitics of the electrodes are already part of an extracted FET model.
Momentum only simualtes passive structures, and what some engineers have done is to model the interconnect up to the active device (gate/etc. electrodes) and then combine the active model with the passive parasitic structure. However, usually the parasitics of the electrodes are already part of an extracted FET model.
"
Thank you!How can I interconnect up to the active device?
Thank you!How can I interconnect up to the active device?