AnsweredAssumed Answered

Multiple Windows Opening on Project startup

Question asked by marc2s on Jul 29, 2009
Latest reply on Aug 26, 2009 by NILESH
I am having a problem in ADS 2009 (but it also occurred in previous versions). When I select the project from the "most recent" list, the project opens up multiple windows of schematics and layouts of all manner of instances and objects used in the design, sometimes as many as 16!. I have tried "close design" before exiting the project, but I still get the same number of windows coming up when the project launches.  

Outcomes