Hi,
I have two branches consisting of an amplifier where the output powers are the same.
At the output of each branch, I added an ideal isolator and define the output impedance as 100 ohm. I then connect the outputs of the two branches together before I connect a 50 ohm load to the common node. By doing so, it seems like I am performing power combining.
Is there anyway I can sum the current instead of the power?
Rgds
Kwang Hwee
I have two branches consisting of an amplifier where the output powers are the same.
At the output of each branch, I added an ideal isolator and define the output impedance as 100 ohm. I then connect the outputs of the two branches together before I connect a 50 ohm load to the common node. By doing so, it seems like I am performing power combining.
Is there anyway I can sum the current instead of the power?
Rgds
Kwang Hwee