Have added custom menus to an ADS DesignKit following the examples in Design Kit Development manual. Now I want to include functions as Place Subnetwork, Open Schematic, Open Display and Show Palette in the menu. Thoose functions are included in the DesignGuide. However when I place a subnetwork I don´t want it to be copied to my project directory.
The DesignKit and menus should work also in ADS2006 (DesignGuides from ADS2004 are not compatible with ADS2006).
The DesignKit and menus should work also in ADS2006 (DesignGuides from ADS2004 are not compatible with ADS2006).