AnsweredAssumed Answered

ICCAP support ed instruments

Question asked by SCUENGR on May 28, 2009
Latest reply on Jan 18, 2011 by Waqas70b
Hi

I would like to use network analyer taking measurements through GPIB interface.  However, the network analyzer model is not on the list of "instrument library."  (I had experience using HP4142 and HP8722 in the ICCAP and know how to make hardware setup in the GPIB section)  

1. Does ICCAP support instruments (specifically for network analyzer) which is not on the list of "instrument library"?

2. What can I do if the network analyzer I tend to use is not in the library?

Thanks for answering.
Calvin  

Outcomes