AnsweredAssumed Answered

Momentum parameterization

Question asked by pschmal on Aug 11, 2010
Hi,

I have a large array structure I am simulating in momentum, 30x30. The structure is parametrized. However, when I change the value of the parameters through Component->Parameters the design does not update. The only way I can get it to update is click individually on the microstrips to open up their properties box, and then hit apply. I don't want to do this 900 times every time I update the parameters.

Usually I place the component into ADS and simulate from there. This time I need to do post-processing and look at the radiation pattern. Unless there is some way to access the radiation pattern data through ADS, which in that case I would be much happier than updating the components in momentum! By the way, why is the radiation pattern data set to a resolution of 1 point per degree? This makes high gain results look ugly and inaccurate.  

Outcomes