AnsweredAssumed Answered

Agilent Connection Expert connecting LAN test equipment

Question asked by lotrsimp12345 on Aug 3, 2010
I have equipment connected to a test bench which is connected on a LAN and has an ip address, I was wondering if there is a way to automatically update this without having to through add interface and selecting the equipment ip address. I would like to do this as part of another install package which uses the AgilentNVisaDrivers. Is there a way to do this preferably through C# by perhaps modifying the registry? It seems to work with GPIB cards but doesn't work with Lan.
Thank.  

Outcomes