AnsweredAssumed Answered

Non-linear model of diode

Question asked by mapin on Jun 10, 2010
Hi,

If I a modelling an SMS7630-079 and I want to have an accurate model for a simulation at 5GHz, do I need to add the package to the model in the Design Parameters>> Artwork?  Will this together with the SPICE parameters of the datasheet be enough to accurately model the diode on Harmonic Balance simulations?

Thanks!  

Outcomes