AnsweredAssumed Answered

Bitwise Operations in Analog Simulation

Question asked by Jcouls29 on Apr 26, 2010
Latest reply on Apr 26, 2010 by Jcouls29
I'm trying to simplify a simulation procedure I have in ADS.  I currently have a good number of Static Switches that need to switch states.  I'd prefer not to have to change every switch state on the fly.  Instead I would prefer typing a single number for the path I want to select (ie. Path = 4) and then use bitwise logic to turn on and off the switches.  Is this possible.  Thanks ahead of time

PS.  The only other option I have is to put together a DAC object with all my possibilities inside it.  I'd also prefer not having to do this.

------
J  

Outcomes