AnsweredAssumed Answered

Momentum Memory Allocation Error

Question asked by MOHEARN on Aug 21, 2006
Latest reply on Aug 21, 2006 by ALEPEREZ
Running a complex Momemtum simulation.

When it gets to the first frequency it stops.  The error is a Memory Allocation Error, it says it has run out of virtual memory.

I'm running on a
Sun SunBlade 1500
4GB Memory
8GB Swap

ADS 2005a
Version: Momemtum MomEngine_64 6.0 2005A.200 June 11 2005
Simulation mode: MW

I've also tried the same project on a Windows2000 machine with lots and lots of memory.  It stops at the same place with the same error.

Is there some thing I can do to correct this?

MO  

Outcomes