What is the "OutFile" option in the Harmonic Balance Bench?
What is written to it?
What format is the file written in?
How can I translate it into something useful?
No documentation.
What is written to it?
What format is the file written in?
How can I translate it into something useful?
No documentation.
[url]http://eesof.tm.agilent.com/docs/adsdoc2004A/cktsimhb/ckhb015.html
Write Final Solution
(UseOutFile)
Check this box to save your final HB solution to the output file. If a file name is not supplied, a file name is internally generated using the design name, followed by an .hbs suffix. If a file name is supplied, the suffix is neither appended nor required. If this box is checked, then the last HB solution is put out to the specified file. If this is the same file as that used for the Initial Guess, this file is updated with the latest solution.
Transient simulations can also be programmed to generate a harmonic balance solution that can then be used as an initial guess for an HB simulation. Refer to Harmonic Balance Simulation.
File
(OutFile)
Specify a file name to save results.
Is this info helpful? Please let us know.
Nilesh 8)