I'm having issues with the Multilayer corner (2-coupled) model. The angle (0 to 90) does not seem to have the expected effect on phase.
For example, small values of angle should result in small values of phase difference, with maximum phase difference at 90 degrees. It does not seem to be working that way (2005A).
Feedback appreciated....
-- Gary Otonari
For example, small values of angle should result in small values of phase difference, with maximum phase difference at 90 degrees. It does not seem to be working that way (2005A).
Feedback appreciated....
-- Gary Otonari
sounds like there are no known issues with the model. a couple of questions to clarify:
the angle limits are 0 to 90 degrees. does 0 degrees mean a straight line, no bend?
the manual states that the model simulates as a "staggered coupled transmission line". so if angle=0, does that mean no staggering, equal lengths?
thx, gary