AnsweredAssumed Answered

Can I control the order that traces appear in list

Question asked by MURPHY294 on Jul 14, 2006
Is it possible to control the order in which traces are arranged in a data display list?  Typically, the traces appear in the order you add them in the plot traces and attributes dialog box, but this isn't always true.  Also there are times when I have created a multi-trace list plot and then I find I would like to add a trace in a specific column of the plot.  The only way I have been able to do this in the past is to delete all traces up to the position of the new trace and then re-add the old traces.  

I haven't been able to find anything in the options.  Is it possible to take control of this formatting?  

Outcomes