AnsweredAssumed Answered

current visualization

Question asked by mantow on Jul 3, 2006
Latest reply on Jul 3, 2006 by ALEPEREZ
Hello, I have done some EM simulations in Momentum for 1GHz to 20GHz. I then try to inspect the currents using the visualization tool. How does one view the currents at a frequency other than the simulation start frequency?

I tried setting Port solution weight so that at 1GHz it is 0, and 10GHz it is 1. But in the main window it still shows:

Shade(DesignName,J)
Freq(GHz):   1


Many thanks.  

Outcomes