Hi,
I tried the example SDFHdlCosim, with Modelsim as vhdl cosimulator. However, I get the message that "Could not load/found the specified procedures: sdfsynthstars, Sdfhdlcosimstars, sdfstars, sdftclstars. These files (.dll, .lib) are all installed in C:\Ads2008\Adsptolemy\lib.win32/lib.win32_64. Is there an environment variable for WinXP or ADS config file which need to be set? I am using WinXP SP2 and also tried it with Filrewall disabled.
Thanks,
R
A sample message:
Simulation / Synthesis Messages
Error detected by hpeesofsim during netlist flattening.
Could not load sdfsynthstars: The specified procedure could not be
found.. Running the simulation from the command line may give a more
detailed error message. See the "Building Signal Processing Models
From the Command Line" chapter of the Ptolemy manual for instructions
on how to do this.
I tried the example SDFHdlCosim, with Modelsim as vhdl cosimulator. However, I get the message that "Could not load/found the specified procedures: sdfsynthstars, Sdfhdlcosimstars, sdfstars, sdftclstars. These files (.dll, .lib) are all installed in C:\Ads2008\Adsptolemy\lib.win32/lib.win32_64. Is there an environment variable for WinXP or ADS config file which need to be set? I am using WinXP SP2 and also tried it with Filrewall disabled.
Thanks,
R
A sample message:
Simulation / Synthesis Messages
Error detected by hpeesofsim during netlist flattening.
Could not load sdfsynthstars: The specified procedure could not be
found.. Running the simulation from the command line may give a more
detailed error message. See the "Building Signal Processing Models
From the Command Line" chapter of the Ptolemy manual for instructions
on how to do this.
Can you run a simpler example, e.g. SineGen connected to a NumericSink, or does this also fail?