Hello,
since a short while, I am sometimes not able to display simulated data using ADS schematic. I found out that the actual reason is that no data file is stored in the data directory of the project. But no error message is displayed.
If this error occurs even restarting ADS does not solve the problem. No I am interested if this is a common ADS bug or how I can investigate or better solve this problem. Any hints are welcome.
I am using ADS 2006 (Update 3) on a Unix system.
Best regards
Mario Leib
since a short while, I am sometimes not able to display simulated data using ADS schematic. I found out that the actual reason is that no data file is stored in the data directory of the project. But no error message is displayed.
If this error occurs even restarting ADS does not solve the problem. No I am interested if this is a common ADS bug or how I can investigate or better solve this problem. Any hints are welcome.
I am using ADS 2006 (Update 3) on a Unix system.
Best regards
Mario Leib
Finally, the mysterious problem is solved: The current ADS version has Problems with 64-Bit computers. At least under UNIX. ADS is not possible to store the simulation data on 64-Bit computers. Why ??? ? I don't know, but I will use it now on our 32 bit machines.
Maybe that's something Agilent should solve
Have a nice weekend,
a frustrated user