AnsweredAssumed Answered

balanced/symmetric input impedance

Question asked by SCHAEFFNER.HARALD.DA on Jun 24, 2007
Latest reply on Jun 25, 2007 by ALEPEREZ
Hello! Have anyone an idea about simulating balanced input impedance? For a S-Parameter Simulation the port have to be terminated with the component term(port impedance). This terminates the input for reflected waves to ground - asymmetric or unbalanced input.
For a between two port impedance the impedance for example Z(1,2) or Z(3,1) must be chosen. Put with a dipole with input impedance between the two ports i don't know where should this termination component should be placed? Between these two ports? A real ground connection is missing! Does anyone know something to this?
Thanks.  

Outcomes