Yesterday, my scope was working fine and now I am getting the following error message:
The system DLL user32.dll was relocated in memory. This application will not run properly. The relocation occurred because the DLL C:\WINDOWS\system32\HHCTRL.oxc occupied an address range reserved for Windows system DLLs. The vendor supplying the DLL should be contacted for a new DLL.
The system DLL user32.dll was relocated in memory. This application will not run properly. The relocation occurred because the DLL C:\WINDOWS\system32\HHCTRL.oxc occupied an address range reserved for Windows system DLLs. The vendor supplying the DLL should be contacted for a new DLL.
RTHDCPL.EXE - Illegal System DLL Relocation
X The system DLL user32.dll was relocated in memory. The application
will not run properly. The relocation occurred because DLL
C:\WINDOWS\system32\HHCTRL.OCX occupied an address range
reserved for Windows system DLLs. The vendor supplying the DLL should
be contacted for a new DLL.
The original patch is described in Security Bulletin MS07-017
http://www.microsoft.com/technet/securi ... 7-017.mspx.
Microsoft has already provided a hotfix to remove the error. The hotifx (KB935448) is at http://support.microsoft.com/kb/935448/. We have tested the hotfix on the DSO80000B and the dialog is gone.