AnsweredAssumed Answered

How do I get an 8 digit frequency value on the 6000?

Question asked by Brig Asay Employee on Mar 21, 2007
Latest reply on Mar 21, 2007 by edgardog
I am reading the manual and according to the datasheet of 6000, if the external 10MHz ref is used with it, up to 8 digits can be counted.

However I can not see the 8 digits frequency value on my MSO6054A. * I use the 53132A's 10MHz out and input from 100MHz to 1GHz by 81134A. I can see the 6 or 7 dights.

How do I count 8 digits?  

Outcomes