If your Infiniium can be connected to the internet.
Go to the Microsoft website, search on Daylight Savings Changing. Then follow the download and install instructions for your geography.
If your Infiniium cannot be connected to the internet.
Follow these instructions to update their Infiniium for the new Daylight Saving Time changes without connecting their Infiniium to a network. Reading the different update articles, multiple countries have been changing: 1. On a computer connected to the network, download the update from http://support.microsoft.com/kb/931836/. Select the "Download the Update for Windows XP package now" link. 2. Copy the Windows XP-KB931836-x86-ENU.exe onto a floppy (for 548xx and 80000A series Infiniium) or a USB thumb drive (for 8000A and 80000B series Infiniium). 3. Insert the update media into the Infiniium. 4. Run WindowsXP-KB931836-x86-ENU.exe on the Infiniium.
Here's instructions for customers who want to update their Infiniium for the new Daylight Saving Time changes without connecting their Infiniium to a network. Reading the different update articles, multiple countries have been changing
On a computer connected to the network, download the update from http://support.microsoft.com/kb/931836/. Select the "Download the Update for Windows XP package now" link. Copy the WindowsXP-KB931836-x86-ENU.exe onto a floppy (for 548xx and 80000 series Infiniium) or a USB thumb drive. Insert the update media into the Infiniium. Run WindowsXP-KB931836-x86-ENU.exe on the Infiniium.
Go to the Microsoft website, search on Daylight Savings Changing. Then follow the download and install instructions for your geography.
If your Infiniium cannot be connected to the internet.
Follow these instructions to update their Infiniium for the new Daylight Saving Time changes without connecting their Infiniium to a network. Reading the different update articles, multiple countries have been changing:
1. On a computer connected to the network, download the update from http://support.microsoft.com/kb/931836/. Select the "Download the Update for Windows XP package now" link.
2. Copy the Windows XP-KB931836-x86-ENU.exe onto a floppy (for 548xx and 80000A series Infiniium) or a USB thumb drive (for 8000A and 80000B series Infiniium).
3. Insert the update media into the Infiniium.
4. Run WindowsXP-KB931836-x86-ENU.exe on the Infiniium.