AnsweredAssumed Answered

error using VXI-11 with v 4.02.0078 DSO6034A firmware rev

Question asked by SemiTech on Jul 11, 2007
Latest reply on Jul 18, 2007 by dnt
Using Linux, I am trying to talk to a DSO6034A oscilloscope using VXI-11 protocol over ethernet.

When I send a standard "*IDN?" command to the oscilloscope, firmware version 04.02.0078, I get back
Error: clnt_create() returned NULL pointer.
main: RPC: Program not registered

This same command succeeds if I am using a DSO6034A with firmware rev. 4.01

Is there an issue with the DSO6000 series firmware?

Thanks.  

Outcomes