I was wondering if there's anyway that the screen image obtained via the web interface for the 6000 series scopes can have the background colour inverted (to white) - equivalent to the "invert graticule colours" option when printing direct from scope to USB stick etc.
Thanks,
Oliver.
Thanks,
Oliver.
Let me suggest something that in reality is not making life easier, but it is relatively simple and quick.
1. You can take a snap shot of your waveform by clicking on the Get Image tab.
2. Once you see the image click on it and you'll see some icons. One of them will be to save it, so save it as .bmp.
3. Open the file and put it on the edit mode.
4. Click on Image/Invert Colors
5. Now you need to make sure it's going to fit on the paper, so click on File/Page Setup and on the Scaling box, there's an option that reads: Adjust to: 50% normal size. You set the percentage, it worked on 50% for me. You can look at the Preview image to see if it's going to fit or not.
6. Print
THis gave me a printout just like when I do it on my USB stick. Perhaps there's an easier way to do this kind of editing. We welcome suggestions.