Hello
Is it possible to run a matlab application on a mso8104a oscilloscope?
The application should only take every fifth measurement from the wavrform. If this is possible please comment or point me to the solution.
Is it possible to run a matlab application on a mso8104a oscilloscope?
The application should only take every fifth measurement from the wavrform. If this is possible please comment or point me to the solution.
runtime library installed on the scope is V75. You will need the
EGUI application to execute a program when the scope application
is up and running. You can install a full version of Matlab on the scope.
There is no built in functionality on the scope to take every fifth
measurement, that I am aware of.