AnsweredAssumed Answered

Question of memory depth DSO3000

Question asked by donpelusa on Jul 24, 2007
Latest reply on Jul 30, 2007 by dnt
Which is the memory depth of the family DSO3000?

If the answer is 4kpts, If sampling in real time a single shot in 1Gsa/s, 1 Channel only.
Wouldn´t I see 4 us of signal? I can only see 80 ns.

If sampling in real time a single shot in 250 Msa/s, 1 Channel only.
Wouldn´t I see 16 us of signal? I can only see 8 us.

If sampling in real time a single shot in 100 Msa/s, 1 Channel only.
Wouldn´t I see 40 us of signal? And I see correctly the 40 us.

My accounts are correct? Why is this happening?

Thanks
Pablo  

Outcomes