AnsweredAssumed Answered

MSO6032A startup problem

Question asked by Pedro80 on Jul 10, 2007
Latest reply on Jul 11, 2007 by Brig Asay
Hello folks!

I was using my 6032A scope normally yesterday and when I came to work and turned it on this morning it acts strangely;
  • It powers up, all lights flash simultaneously (also the LCD flashes)

  • All the LED's start to light up in sequence (this complies to what is described on page 85 in the service guide of 6000-series)
 
The problem is that the LCD does not light up at all(!) The "Single" button stays lit (after the light sequence) for about 20sec, then the light sequence starts all over (only change is that the now it loop continuously without the "Single" button staying lit..).

Anyone got some kind of clue what could be the cause of this?
I have no idea, I've tried powering off and on, with and without probes connected, theres no contact through USB or LAN and no buttons seem to work..  

Attachments

Outcomes