Dear Friends
I have already raised the problem of infiniium 80204B is not connected to 89601A VSA, but the problem exists.
Problem detail is,
1. Infiniium 80204B Oscilloscope.
2. VSA used: version 6.x and 9.x (licensed versions)
3. Options 200 and 300 are purchased.
4. When VSA is loaded, a Warning message is displayed: "Cannot find a support input .Input will simulate an Agilent VSA E1439 70 MHz IF 95 Ms/Sec ADC"
5. Factory installed Version was 6.x.
6. I installed the free updates from Agilent which is 9.x.
7. During installation the option of "Hardware Support" was grayed (disabled).
8. I executed Agilent connection expert
9. I clicked on GPIB0 it displayed the following,
VISA interface ID. GPIB0
Serial number MY12345678
GPIB address 21
System controller YES
SICL interface gpib0
Logical Unit 9
Board number 0 (GPIB0)
Auto discover YES
Please guide me to resolve the problem so that maximum utilization of the equipment is made and my investment is not wasted.
Regard Fahim
I have already raised the problem of infiniium 80204B is not connected to 89601A VSA, but the problem exists.
Problem detail is,
1. Infiniium 80204B Oscilloscope.
2. VSA used: version 6.x and 9.x (licensed versions)
3. Options 200 and 300 are purchased.
4. When VSA is loaded, a Warning message is displayed: "Cannot find a support input .Input will simulate an Agilent VSA E1439 70 MHz IF 95 Ms/Sec ADC"
5. Factory installed Version was 6.x.
6. I installed the free updates from Agilent which is 9.x.
7. During installation the option of "Hardware Support" was grayed (disabled).
8. I executed Agilent connection expert
9. I clicked on GPIB0 it displayed the following,
VISA interface ID. GPIB0
Serial number MY12345678
GPIB address 21
System controller YES
SICL interface gpib0
Logical Unit 9
Board number 0 (GPIB0)
Auto discover YES
Please guide me to resolve the problem so that maximum utilization of the equipment is made and my investment is not wasted.
Regard Fahim