AnsweredAssumed Answered

SOLT

Question asked by JrV on Oct 9, 2009
Latest reply on Nov 13, 2009 by Hemanthkumar
Hello,

I am using an PNA-L N5230C option 146 and 080

I have the following setup:

Two external couplers.
The coupled lines are connected via an attenuator (for protection and not to go in compression) to the measurement receiver A, B, C and D.

I like to perform a full 2 port cal using SOLT.

Do I need to implement the calibration routine?
If yes, what is the way to do it?
Some extra info plus guidelines are welcome.

Regards,
J.  

Outcomes